Deletes an array of objects in the project
The response body is of type RunningStatusGetResponse.
The running status of the CIMPLICITY project.
Overview
 |
RunningStatusGetResponse
The running status of the CIMPLICITY project.
 |
IsProjectRunning : boolean
represents the CIMPLICITY project is in run mode.
|
 |
IsPrimaryRunning : boolean
represents the CIMPLICITY Primary node is in run mode.
|
 |
IsSecondaryRunning : boolean
represents the CIMPLICITY Secondary node is in run mode.
|
 |
IsStartAtBoot : boolean
indicates if the project is configured to start at boot.
| |